Cancel
Showing results for 
Search instead for 
Did you mean: 

Pattern a curved extruded part

Pioneer
Pioneer

Hey

 

I try to figure out a way to pattern a part along a vertical line which is extruded along a curve. If I use the command pattern and select the part and the vertical line then Solid Edge does something, but It looks like a real mess.

 

It is posible to pattern the curve which the part is extruded along and then extrude the same profil along these lines. But this would take forever.

 

I upload a picture "This is the wanted result" where you can see what my goal is and a .prt file where I try to achieve it. It would help me if someone can explain what Solid Edge does in this .prt file, too.

 

Sincerely Michael

18 REPLIES 18

Re: Pattern a curved extruded part

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@MichaelVoelz  I could fix it by switching to the "Fast" option, but the way the "Smart" option does it is wierd...



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com

Re: Pattern a curved extruded part

Genius
Genius

Hi @MichaelVoelz Is this the result you want?

Pattern a curved part.jpg

Re: Pattern a curved extruded part

Pioneer
Pioneer

@KennyGYep, you are right. It is fixable with the "fast" option. Thanks.

 

@KanwulfThats exactly what I want. Did you do it the same way via "fast" option?

Highlighted

Re: Pattern a curved extruded part

Genius
Genius

Hi @MichaelVoelz Yes, with the "fast" option the problem is solved.Smiley Happy

Re: Pattern a curved extruded part

Pioneer
Pioneer

Okay, thanks for the answers. It works for this specific part.

 

Is someone able to tell me why an error occurs when I try the EXACT same thing in another part. I try to pattern "Ausprägung 18" along the vertical line  in "Skizze 6". I upload the part which I am talking about.

The error just says "no pattern created" or "process failed".

 

The pattern will cut the screw, but this shouldnt be the reason for the error...

 

Or maybe is there an easier way to extrude a curved part vertically without using pattern? (pic)

Re: Pattern a curved extruded part

Genius
Genius

Hi @MichaelVoelz Try it with “ Pattern Intelligent”

 

Thanks.

 

Regards.

Re: Pattern a curved extruded part

Pioneer
Pioneer

@KanwulfThe error occurs with pattern smart an pattern fast unfortunately .

Re: Pattern a curved extruded part

Genius
Genius

@MichaelVoelzSo weird...Spindel50x10.jpg

Re: Pattern a curved extruded part

Pioneer
Pioneer

@KanwulfHow did you get this result showing in the picture ?

 

I thought the error occures because the sketch which contains the vertical line is in the syncronous modus. So I rebuild the part with only sequentiell elements. But the same error pops up by pattern the curved element.

 

It is possible to pattern the whole part (screw+curved element) along this vertical line the way I want it. But I can only do 5-10 pattern, if I try to do more Solid Edge tells me 15min+ that the pattern will be created without any result.

 

Any ideas ?