Cancel
Showing results for 
Search instead for 
Did you mean: 

Pattern by table brake link

Pioneer
Pioneer

Hello, I would like to know if there is any way to brake the link of the pattern by table to the excel so it's dropped.

 

Why I need this is because the PLM software that I use can't support the excel file.

4 REPLIES

Betreff: Pattern by table brake link

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hi Norbert,

 

If you create the pattern by table you can uncheck the "Link" Option2016-11-11 15_54_03-Instance Table_.pngInstance Table

 

If you have already created the pattern it is also possible to break the link.

 

Via ApplicationMenu--> Info--> Edit Links

 

2016-11-11 16_01_33-Solid Edge ST9 - Synchronous Part - [Dateiname].png

 

But this will also delete the Pattern..... (That was the behaviour to me)

 

So i made it again and uncheck "Link"

 

I tested this in Synchronous Mode

 

Hope this helped you

 

 

Betreff: Pattern by table brake link

Pioneer
Pioneer

I am actually missing that link option

Betreff: Pattern by table brake link

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,



supoose You don't use ST9

 

This option was implemented in ST9



regards
Wolfgang

Betreff: Pattern by table brake link

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Yes you are right i am using ST9.

 

Probably a reason to upgrade to ST9.

 

Greetings Christian