Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Pattern quantity on callout

Valued Contributor
Valued Contributor

how can i get a callout to show the quantity of a pattern, non hole patter. 

So for example i have a part with a rib that has been circular patterned. on my drawing i would like to show the quantity of this rib using a callout. 

 

 

Regards,

MagRiz
(ST9 User Est 01.18)
9 REPLIES 9

Re: Pattern quantity on callout

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Don't believe you can.  I think Holes are the only feature that use the automated feature count.



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com

Re: Pattern quantity on callout

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You can format a callout to show quantity using "parts list quantity" under graphic connection.

PL_Qty.png

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Pattern quantity on callout

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

Absolutely Yes. These parameters will be available in Variable table. You have to toggle on it and that's all.

 

Here is a video:

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: Pattern quantity on callout

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Imics  That's an excellent workaround!  Just expose the variable and then use Property Text to pull it.



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com

Re: Pattern quantity on callout

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Imics

 

But this only will work for curved patterns directly and only if there are no suppressed occurrences for that pattern.

I assumed that the initial request more goes into the direction of knowing how many active pattern instances there are.

 

 

regards
Wolfgang

Re: Pattern quantity on callout

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I think my answer above was mismarked as the solution. It seems like @Imics' post should be the solution.

Upon rereading this thread I realized I goofed and interpreted the question as an assembly drawing issue when it was actually a part drawing issue.

Can you double check @MagRiz?

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Pattern quantity on callout

Valued Contributor
Valued Contributor

@bshand

 

Thats correct. thanks for spotting it. 

Regards,

MagRiz
(ST9 User Est 01.18)

Re: Pattern quantity on callout

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Can you uncheck mine? IDK if that's possible or not.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Pattern quantity on callout

Gears Phenom Gears Phenom
Gears Phenom

@bshand, my solution is your solution too, no problem. Smiley Wink

@hawcad, it seems this helped @MagRiz. Smiley Wink

 

BR,

Imics
http://solidedgest.wordpress.com/