01-11-2018 01:42 PM
We have a customer that is running ST9 MP10.
When they pattern a component in an assembly it turns on th planes in all the patterned parts.
Not the original, just the copies.
Various pattern type behave this way. More than one user.
I can't reproduce.
Anyone have this happen?
01-11-2018 03:24 PM
The patterned parts follow the same rules as newly inserted parts. There are switches somewhere that determine if sketchs and planes, etc are turned on or off when they are inserted into the model.
01-11-2018 03:52 PM
I think that in solid edge options, under Assembly, if you go down to construction display options, if you check the "show reference planes of component, and then select the "hide after placement" option it ight remedy this.
01-11-2018 03:53 PM - edited 01-11-2018 03:55 PM
@12GAGE, @nominus38, That's not so when I do it. Patterns don't follow those settings.
01-11-2018 03:58 PM
If that isn't it, then what is it. Does it place everything with whatever it's last saved display settings were for the particular component? I do agree with 12Ga as there is somewhere you tell it to do this behavior, I just don't remember exactly where that is...
01-11-2018 04:10 PM
Okay I figured it out. Uncheck "Patterned parts inherit parent part occurence properties by default. Then it will stop.
01-11-2018 04:15 PM - edited 01-11-2018 04:18 PM
Actually, check that, I'm going back to my original answer. But you have to be inside of the the component that is getting patterned, then go into the options, then change that setting to hide reference planes after placement. Then you when you pattern that component, it won't show the reference planes after patterning.
beforeafter01-11-2018 04:26 PM
Okay, i actually figured it out. Go into the component that is getting patterned, and uncheck all of it's reference planes, even if "reference planes" is unchecked. You need to uncheck them individually, then save. This will fix
01-11-2018 04:26 PM
I couldn't follow what you did. Need to have video show all of SE. Or I'm just thick.
01-11-2018 05:55 PM
All I did was select the pattern function. Everything else is on screen. Oh and I saved. And backed out to the higher level assembly. There wasn't much going on off screen.