Cancel
Showing results for 
Search instead for 
Did you mean: 

Patterning in assembly using cutouts

Gears Phenom Gears Phenom
Gears Phenom

Hello,

 

I have an assembly with a small tab that is constrained to a rectangular cutout in a channel.  There are several rectangular cutouts in the channel and I would like to pattern the tab using the cutouts.  The cutouts are not evenly spaced and as far as I know, ST9 won't pattern using cutouts.  Fortunately, I have hole features that are on the same channel that follow the same spacing.  I was able to use the holes to "trick" SE and pattern the tabs.  What are the prospects of ST10 being able to pattern on other features besides holes?

 

Kyle

 

 

Kyle Joiner
IPA LLC
ST10 MP1
3 REPLIES

Re: Patterning in assembly using cutouts

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Smiley Very Happy

 

https://community.plm.automation.siemens.com/t5/Solid-Edge-Blog/What-s-New-in-ST10-Clone-Components/...



Ken
Production: ST10 MP7, Testing: SE 2019
http://Grundey.blogspot.com

Re: Patterning in assembly using cutouts

Gears Phenom Gears Phenom
Gears Phenom

I think that's exactly what I'm looking for.  If I'm reading it correctly, the Duplicate command is used to find matching occurances and Clone is used to find matching faces.  That's pretty cool!

 

Kyle

Kyle Joiner
IPA LLC
ST10 MP1

Re: Patterning in assembly using cutouts

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @kjoiner

 

 

 

but You can use the ST9 functionallity of duplicate features and parts using blocks in sketches.

 

If You create the cutouts in Your part using the ducplicate by blocks of a sketch (or more sketches in different planes) then You can use the same function for duplicate Your parts in the assembly.

 

I see this as real good function.

 

 



regards
Wolfgang