Cancel
Showing results for 
Search instead for 
Did you mean: 

Peer Command Command Bar will Not Open

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

Working On This Project That Requires The Peer Command...

Open Up Assembly

Sketch > Tool > Edge Locate > Peer Command... First Attempt Worked Great... After That The Peer Command Will Close And Open But, The Command Bar Will Not Show.

Go Over The Same Steps And The Sketch Command Bar Always Shows But, Not The Peer Command Bar... 

I've Even Restarted No Luck

 

Thanks

GregoryLee

 

 

1 REPLY

Re: Peer Command Command Bar will Not Open

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@PO_LC , there is no Command Bar associated with the Peers command.  That is an option toggle that turns off/on the ability to locate "peer geometry" or geometry of other parts in the assembly.



Ken

Production: ST10 MP7
Testing: SE 2019
http://Grundey.blogspot.com