Cancel
Showing results for 
Search instead for 
Did you mean: 

Peer Variable Question

Gears Phenom Gears Phenom
Gears Phenom

Hi Edgers,

 

I wonder if someone of you knows the answer ;-)

 

I am trying to understand how to change the formula when I am pasting the link to another part dimension.

 

Variable inquiry.png

 

The variable V453 is linked to a different part which it has a width 400mm.

What I want to achieve is a formula like - (@ link to another part dim) - 3mm - so, in conclusion, I will get 397mm.

 

Would you please tell me how to write that formula?

 

thanks,

Arek

 

 

3 REPLIES 3

Re: Peer Variable Question

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hi Arek:

  

It seems you cannot directly edit CopyLink-PasteLink formula.

 

Instead ceate a new var and PasteLink the width from another part into the var.

Then use the var in the (final dimensions) - 3

  

The following image shows the steps:

 

CopyPasteLinkFormula.png

Hope you find this useful.

 

Regards,

Tushar

wwwSurfAndCode.IN

 

Re: Peer Variable Question

Gears Phenom Gears Phenom
Gears Phenom

Hi @Tushar

 

 

You are The STAR Tushar. Thank you.

 

Regards,

Arek

Highlighted

Re: Peer Variable Question

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Thanks for the praise Arek.

That was a low hanging fruit.

 

In fact, it is a recommended practice to always inter-link to local variables and then use those variables to drive dimensions. This way they can be kept separate and formulas can be applied before using the values.