Cancel
Showing results for 
Search instead for 
Did you mean: 

Place dimension automatically

Phenom
Phenom

I work in ordered.

 

When sketching you can input the value of a line, circle,...

After confirming the sketch has the correct size, but the sketch has no dimension.

 

I think I saw an option once in SE to place this dimension automatically when you input a value but can't find it.

 

Someone who can help?

...........................................................................................................
Solid Edge 2019 & AutoCAD 2019 user
4 REPLIES 4

Re: Place dimension automatically

Experimenter
Experimenter

Hey,

 

If you go to Home -> Dimension -> and activate Auto-dimension, this should do the job.

 

 

Re: Place dimension automatically

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Joris,

 

What you want is in Intellisketch Options....

 

ST8_IntellisketchOptions.png

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Place dimension automatically

Phenom
Phenom

@SeanCresswell Yes!, That's it.

 

Thanks Man Wink

...........................................................................................................
Solid Edge 2019 & AutoCAD 2019 user

Re: Place dimension automatically

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

No problem @Joris....glad to help.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000