Cancel
Showing results for 
Search instead for 
Did you mean: 

Point of view? Not sure what else to call it.......

Legend
Legend

So, I have a large assembly, and I'd like to get a view from inside, using a standing person model as the point of view. How, if possible, would I go about doing something like this? Maybe this isn't something SE can do?

1 REPLY

Re: Point of view? Not sure what else to call it.......

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
You have to turn on the view Perspective, and then you can zoom inside a model and should be able to rotate about the camera position inside the model.


Ken
Production: SE 2019 MP4, Testing: SE 2020
http://Grundey.blogspot.com