Cancel
Showing results for 
Search instead for 
Did you mean: 

Preview in feature library?

Valued Contributor
Valued Contributor

I've made a few feature libraries ...
I do not know what this is ...
Not available in preview format?

Below is a preview of the feature library on SolidWorks.
Can Edge be provided with this?
This feature saves a lot of time.

feature libruly.png

 

Below is the screen of the edge.
Where can the preview be?

edge Feature.png

6 REPLIES 6

Betreff: Preview in feature library?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Hclee

 

 

 

go to the pathfinder, click the right mouse button and activate the Preview!

 

 

This will open an extra preview form in the pathfinder, showing the feature similar to the parts in assembly pathfinder

 

 

regards
Wolfgang

Betreff: Preview in feature library?

Valued Contributor
Valued Contributor

I've enabled preview but ...
The feature library looks unlikely to appear.

It looks too big or too small.
It does not distinguish.


Could you show me the process ...?

Betreff: Preview in feature library?

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Further to what @hawcad said, there is a option to show the thumbnail:

 

PreviewFL.png

Betreff: Preview in feature library?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Tushar

 

 

 

thanks, forgotten to mention that!

regards
Wolfgang

Betreff: Preview in feature library?

Valued Contributor
Valued Contributor

hi ~ Tushar
It has a large icon ...
And the feature library does not appear.

Nothing is displayed.

ss1.png

It's not a part
It is a feature. The feature library can not be previewed.

Highlighted

Betreff: Preview in feature library?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Hclee

 

 

 

Yes @Hclee

 

 

the library too can be shown in preview and thumbnail mode

 

20170918_1522.PNG

regards
Wolfgang