Cancel
Showing results for 
Search instead for 
Did you mean: 

Printer Settings

N/A

Hi,
Does soild edge 2d over ride the printer settings on your printer driver when printing.
I am looking to purchase an epson photo stylus printer ( model 1400 - 13" wide format
) for an allround printer and was wondering how print outs would look like from
solidedge free 2d.
Thanks,
Jason
1 REPLY

Re: Printer Settings

N/A
Jason,
There are program specific settings that are listed when you print. There
are also printer specific settings that you may get to based on the printer
selected in the print dialog. To get to the printer options, click on the
Properties button next to the printer selected. Solid Edge will maintain the
program specifis settings, but not the printer specific ones. The same
printer may be used by multiple programs.
Regards,
Rick B.