Cancel
Showing results for 
Search instead for 
Did you mean: 

Printing Problems

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hi edgers!

I have a problem when I try to print a .dft. This problem only happen in a format bigger or equal to DIN A3.

When I select print, I have this configuration in the print options (see screenshot 1).

 

Print options.jpg

 

When I print it, appear the paper in vertical and the draft in the middle of the paper scaled.

If I try to export the same draft in pdf I have the same result. There is any configuration that I need to change? Or maybe it’s a register problem?

 

Thanks,

1 REPLY

Re: Printing Problems

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I think you need to fiddle with the printer settings as well.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200