Cancel
Showing results for 
Search instead for 
Did you mean: 

Printing command crashes system

Not applicable

Everything working fine but if I try to print it says memory low,Crashes!
Even a very small drawing.
Running as ADMIN, No problems with other CAD and graphic programs (Very large/copmplex)
Oh well, was worth a try.
OS Name Microsoft® Windows Vista™ Ultimate 64BIT
Version 6.0.6001 Service Pack 1 Build 6001
HP-Pavilion d5000t x64-based PC
Processor Intel(R) Core(TM)2 Quad CPU Q9450 @ 2.66GHz, 2667 Mhz, 4
Installed Physical Memory (RAM) 6.00 GB
2 REPLIES 2

Re: Printing command crashes system

Not applicable
John,
Solid Edge produces a crash log when a crash occurs. There are two files,
crashlogf.txt and crashlogf.dmp. These can be found in the "C:\Documents and
Settings\YOUR LOGIN\Local Settings\Temp" folder. If you will send these
files to me, we can try to see what caused the crash.
Regards,
Rick B.

Re: Printing command crashes system

Not applicable

"Ricky Black" wrote:
>John,
>Solid Edge produces a crash log when a crash occurs. There are two files,
>crashlogf.txt and crashlogf.dmp. These can be found in the "C:\Documents and
>Settings\YOUR LOGIN\Local Settings\Temp" folder. If you will send these
>files to me, we can try to see what caused the crash.
>
>Regards,
>Rick B.
>
>

Thank you for response to my Print/Crash problem.
I have nothing anywhere on my PC with those file names.
As I stated just clicking "Print", I get a "Low memory error" then program crashes.(
Not Windows).
Only crashes on this PC so far is Solid Edge.
Could be Vista/64: I'm it in running X86-as Admin though.
Tried different settings but no help. It's only related to attempt to print. Interesting!