Cancel
Showing results for 
Search instead for 
Did you mean: 

Problem on solid edge ST9 3D Modelling (Part, sheet metal, Weldment and Assembly)

Experimenter
Experimenter

Hi,

I have used ST9 and i have an visual issues as attached Photo. it is repeatedly coming while using comments in Part, Assembly, Sheetmetal. 

Kindly help.

1 REPLY

Betreff: Problem on solid edge ST9 3D Modelling (Part, sheet metal, Weldment and Assembly)

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Dinesh_Kumar

 

 

this is a graphic cards issue and maybe a question of driver and/or options in SE.

 

Which graphics card do You use?

 

Try to change the graphics mode in SE via Options - View and Application Display 

 

 

20170506_0821.PNG



regards
Wolfgang