Cancel
Showing results for 
Search instead for 
Did you mean: 

Problem opening Parasolid Files

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hello!

 

I have a problem openning Parasolid Files. 

I convert it with the ST9 MP8 without problems, then, when I tried to open it the program shows and error:

The output file does not exist or does not have writing permition. Select another output file. (Directly translate from Spanish "la carpeta de salida no existe o no se dispone de permisos de escritura. Seleccione otra carpeta de salida").

It happens with all my parasolid files and I dind't change any file name. 

 

¿You may have any idea?

2 REPLIES 2

Betreff: Problem opening Parasolid Files

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

HI @cst-prismacim-effort

 

 

 

try to change the options for input.

Could be that You do not have any write permissions to the folder where the results should be created.

 

Another approach, I use in such casses is, to rename the CurrentUser entries for Solid Edge to see, wether or not my settings are corrupt.

 

Or You login in with a different user name, to test the same

 

regards
Wolfgang

Betreff: Problem opening Parasolid Files

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hi Wolfgang

 

The user have all the write permisions to the folder. That folder is saved into the desktop. The day before to that issue was possible to open and save the files without problems. 

 

How can I rename the CurrentUser for Solid Edge?

 

Thank you and best regards.