Cancel
Showing results for 
Search instead for 
Did you mean: 

Problem to run Solid Edge ST9 Student Edition

Creator
Creator

Hello.

I have a problem to run Solid Edge ST9 Student Edition.

When I run the program, this don't open and show an error. See image.

 

I have Windows 10, Version 1511, 64 bits, processor Intel Core i5 and 4 Gb of RAM.

 

Thanks for your help.

 

Regards,

Diego

 

 

12 REPLIES 12

Re: Problem to run Solid Edge ST9 Student Edition

Experimenter
Experimenter

Did you get this fixed?

Re: Problem to run Solid Edge ST9 Student Edition

Creator
Creator

Hi JEvans.

I can´t use solid edge for this issue.

Highlighted

Re: Problem to run Solid Edge ST9 Student Edition

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hi,

this is general error window when "something unusual" happens.

 

I recommend:

1. Upgrade graphics card driver

2. Check if there are any pending Windows Updates

3. Reinstall Solid Edge

 

At the bottom of error window there is a path to crashlog.txt file. Can you post it here?

 

Ota

Re: Problem to run Solid Edge ST9 Student Edition

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

In the error dialog it lists a crash log file at the bottom.  Find that file and post it here.  May provide some clues.  Does this happen if you attempt to load a DFT file?



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com

Re: Problem to run Solid Edge ST9 Student Edition

Creator
Creator

Hi.

Thanks for your help and I'm sorry for my delay in answer but I was very busy in my work and university.

I attached the file "crahlogf.txt" for your help.

 

Thanks a lot.

 

Regards,

Diego

Re: Problem to run Solid Edge ST9 Student Edition

Creator
Creator
Hi ota_poul2.
I followed your recomendations but I still have the problem.

Thanks for your help.

Diego

Re: Problem to run Solid Edge ST9 Student Edition

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

 Hi,



the next step I would try is, to uninstall Solid Edge completely and then install it new but not under c:\programms rather ontoory  a second disc or second partition where You creat a new directory (could also has the name programs) and start it from there.

 

I have seen rights problems when not enough privileges are available for the user

 

regards
Wolfgang

Re: Problem to run Solid Edge ST9 Student Edition

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Interestingly enough the crashlog does not list any PC specs...  This doesn't happen to be installed on a MAC running BootCamp or Parallels (or other desktop virtualization for a Mac)?

 



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com

Re: Problem to run Solid Edge ST9 Student Edition

Creator
Creator
Hi Grundey.
I'm using Windows 10 and not IOS of Mac.

Thanks

Diego