Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Problem when open dwg files

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Not seeing the problem with ST8 latest MP

So it seems the freezing after zooming problem has crept in with ST9 or just the latest MP you applied.

 

Re: Problem when open dwg files

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Yes. This promble is only my computer. and Is not big Isue. I would like to ask if anyone has this problem.

I'm test fix;

 - Remove SE and Registry

 - Update Graphic card

 

Re: Problem when open dwg files

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Famer

 

 

just opened that DWG and there are no problems with ST10

 

And I know this DWG for many years now, have opened and translated it many times on many computers and I can not remember to had any issue together with this draft file.

 

And to be honest, this is such a small DWG that it is hard to imagine to have any problems with it.

 

 

Before uninstalling Solid Edge from Your computer, try to change the user first, so You can verify wether or not there are problems with Your user settings, options, rights etc.

 

 

And also try to rename/delete the entries for Solid Edge in the Current User registry and in %appdata%

So You can test wether a new default SE setup will have this issues too.

 

And, since it is a DWG import, check Your INI settings for this import.

Maybe there are wrong options set.

 

 

regards
Wolfgang