Cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with ADD-IN in ST9

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hi,

 

I have created the default add-in using visual studio..when I execute 

register-solidedgeaddin

 I get the addin in the addin manger but it's not displayed on the ribbon.

I'm using ST9 , SolidEdge.Community.AddIn 108.0.0 and Interop.SolidEdge 109.1.0..

 

Any help.

Best Regards.

Amani BILEL

1 REPLY

Re: Problem with ADD-IN in ST9

Esteemed Contributor
Esteemed Contributor

Please post to the Solid Edge Developer Forum... They will be better suited to answer this question.

 

My guess if you are seeing it in the add-in manager but not the ribbon is that your code did not properly add it to the ribbon as it appears it is registerd.



Ken

Production: ST10 MP5
Testing: SE 2019