Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Problem with SE2019 and MP07

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@hawcad Based on what I see of a working version, with the Select command active and Closing the Sketch, the Select command bar disappears while the Profile Error Assistant dialog is present and only reappears after the dialog is closed.

 

In the MP7 version, the Select command bar reappears almost immediately after closing the sketch which leads me to believe the Profile Error Assistant dialog is not displayed anywhere.



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com

Re: Problem with SE2019 and MP07

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @KennyG 

 

 

what I have seen now is, that - I have moved the pathfinder away from the left side - and can see a very short appearance of a form window (suppose according to the size this is the error wizzard) without showing or seeing any text etc.

 

I have found an entry in the registry called FontName for ProfileErrorAssistent

 

This value was empty, and I tested with arial:

 

20190522_1721.png

 

But doesn't change anything.

Furthermore I have taken a look into an old version of my registry files and they are identical in that area.

 

 

regards
Wolfgang

Re: Problem with SE2019 and MP07

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Sorry @hawcad ....I re-read the crux of the issue.....and have now repeated this issue.

I'd suggest logging an IR.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Problem with SE2019 and MP07

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi @hawcad ,

 

Same behaviour here. I found a trick to work until they solve this. First draw the sketch with the sketch commands, and then, use the protusion tool. If you have an open sketch, with this workflow it will show the error.

 

Another option is to downgrade the manteinance pack...

 

Regards,