Cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with Solid edge license

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

There is a problem in Solid edge ST6 , it was a network license & frequently getting problem with license. The license was configured in server with license manager tool and it showing as "license file not found" in client machines some times. and it was resolved after manual configuration of LM tools, can any one please help me to understand what will be the reason for this problem

2 REPLIES

Re: Problem with Solid edge license

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Not sure if this is your issue, but if you are running over a slow network (WAN, VPN), the timeout on the clients for gettng a license is too short and will often give up and post a message stating the license can't be found.  to fix, follow the steps below.

  1. Go to Control Panel, System (or right click on Computer and select "Properties").
  2. Click "Advanced system settings" (may need admin to do this)
  3. Select the "Advanced" tab
  4. Select "Environment Variables"
  5. In the "System variables" section, select the New... button
  6. The variable name will be "FLEXLM_TIMEOUT" and the value will be "3000000".

This will provide Solid Edge with 3 seconds to contact the license server and get a response.  If this does not resolve your issue, then it is probably something else.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: Problem with Solid edge license

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer
Thank you Mr.Ken Grundey