Cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with Standard Parts on ST9

Experimenter
Experimenter

Hi,

 

I have a problem with the standard parts installation. I have the SolidEdge ST9 Student Version.

When I try to open standard parts in SE, I get a error message saying "Standard Parts is not configured correctly, check Application Menu...".

After reading some posts, I figured that I might have to run the StdParts.exe file. But that file doesn't seem to work.

Could anyone please help on this issue?

 

Thanks,

Chock

1 REPLY 1

Re: Problem with Standard Parts on ST9

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hi,

you need to launch Configuration Wizard and set paths similar to those:

 

Configuration Wizard.jpgDefault paths for Standard Parts installed locally

 

After setting, click on Save and there should be message that configuration file .SAC was created. 
Then open Solid Edge, open new assembly file, go to Options and in File location Tab you need to define where is location of .SAC file:

Location of sac file.jpgOptions Solid Edge for Assembly environment