Cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with Sweep

Experimenter
Experimenter

Hello

 

I have followed this tutorial:

https://www.youtube.com/watch?v=IuCb49_tQAc

 

When I get to the 19. min, a sweep, I get errors (see attached *.png). It seems there is sth wrong with the sketch circle prior to the bend?

Part file attached

 

- Could anyone tell me what's wrong?

8 REPLIES

Re: Problem with Sweep

Phenom
Phenom

Hello,

I think the difference between you and the procedure of CAAP is that they checked in FACE CONTINUITY "CURVATURE CONTINUOUS".

Yasser

Re: Problem with Sweep

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

changed to TANGENT CONTINUES

Re: Problem with Sweep

Phenom
Phenom

sweep_01.jpg

Re: Problem with Sweep

Experimenter
Experimenter

Hey

 

Thanks for replying. I didn't add that i tried a couple of different combinations, including of course the 'tangent' according to the tutorial but I still get the same error.

 

Whan i apply the sweep it says that the sketch has intersecting contours. So I lowered the diameter of the sketch from 24 to 10 mm.

Attached the result. Sth's wrong!!

Re: Problem with Sweep

Phenom
Phenom

Hi,

I tried it and it works fine.

I don't know if you speak Nederlands...

[De doorsneed wordt uit verschilende elemente opgebouwdt en sketches hebben groune line/elemente "minute 21"]

the sketches are build from more than one line to be able to pick them during the sweep proecedure.

 

Re: Problem with Sweep

Experimenter
Experimenter

No, that's the other thing. I'm Danish. I understand it superficially..

 

So what did you do to succeed with the sweep? I also tried the multiple sketch sweep but it didn't work neither. It seems like the sketch on the bend (sketch 16) causes the problem because I can sweep between the first four sketches but not #16

Re: Problem with Sweep

Phenom
Phenom

The sketches are build from more than on line.

Try to get the same view like in the video to be able to pick up the right segment of the line and I hope you will.

I think you achieve it...

Re: Problem with Sweep

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

Hello,

the problem is not with sketch #16 but with the very first one #1.

 

The bottom line on this was parallel with the plane baseline but not attached to it.  You can go back to this sketch and delete some of the relationships and then try to get it so that the small line (0.2) is horizontal with the plane base line. 

 

Once you've done that you may need to reattach the next sketch 2.  I tried this and it worked okay as below:

HandlebarPicture.png

Cheers,

 

Frank

 

Edinburgh University