Cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with assembly after installing ST8

Experimenter
Experimenter

Hi everyone,

 

I am working with Solid Edge at work and I am having a problem when I make an assembly with subassemblies after upgrading to ST8

 

When copying a subassembly (because I need 2 of them in the compleat assembly) the parts get copied, but change the subassembly.

So when I open the original subassembly, the parts are doubled in there.

 

Are there any functions I need to adjust and if so, where?

Can somebody help?

 

thanks,

Joowan

 

1 REPLY

Re: Problem with assembly after installing ST8

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there,

 

I don't get that problem....I can drag in another instance of a sub-assembly as many times as I want, with no issue. [4 subs in the below image....]

 

ST8_ASM_Multiple Sub-Assemblies.png

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x3 seats]
Windows 10 - Quadro P2000
Testing: Solid Edge 2019