Cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with bending of face

Experimenter
Experimenter

Hello everyone,

 

I just started with solid edge a few weeks ago. I have done all the standard solid part tutorials.

 

As an exercise i was trying to model a skateboard. I designed the flat board (see picture). Now i'm trying to bend both of the ends a bit, so it looks like a real skateboard. I've been searching for a while now, but i cant find a way to do this. Is there nowhere like some sort of "bend face" command?

 

The flat 'skateboard':

bord.JPG

Curvature i would like to give the ends:bordbend.JPG

10 REPLIES 10

Re: Problem with bending of face

You might consider the sheetmetal envoronment... for true bends.

 

Or in part just draw you profile with the desired bends befor you extrude.

 

or since you now have that surface you can "replace face"

 

I think the best approach is to modify the originating profile. (if in orderd)

 

 

Highlighted

Re: Problem with bending of face

Phenom
Phenom

Just to add to Matts comment about sheet metal - you can switch to the sheet metal commands within a part file.

Then you should be able to apply a bend to the end of the part.

You will pobably have to remove the edge rounding first.

HP Z420 16GB RAM
Quadro K4000
SE2019 MP5 on Windows 10 Pro 64.

Re: Problem with bending of face

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there,

 

Not sure what version of SE you're running, but...you could also go about this in a different way.

Maybe try using "Cross Curves" from 2 intersecting sketches to generate a surface, which can then be thickened.

 

See my "very quick & rough" process below [in ordered mode].... [I can provide this file, if you have ST8 installed]

 

Top view sketch profile.

ST8_PAR_CrossCurve_Skateboard Deck_A.png

 

Front view sketck profile.

ST8_PAR_CrossCurve_Skateboard Deck_B.png

 

Cross curve command. [found on the Surfacing tab]

ST8_PAR_CrossCurve_Skateboard Deck_C.png

 

Create a "Bounded" surface of the cross curve.

ST8_PAR_CrossCurve_Skateboard Deck_D.png

 

Thicken the surface to the desired amount.

ST8_PAR_CrossCurve_Skateboard Deck_E.png

 

Turn off the features in the pathfinder to see the result only, and apply your edge fillets.

ST8_PAR_CrossCurve_Skateboard Deck_F.png

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Problem with bending of face

Legend
Legend

Sean,

 

I tried to make something using the method you just showed and I had an unexpected outcome. The object seemed to normalize to the curve instead of staying flat to it?

Re: Problem with bending of face

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@nanan00 wrote:

Sean,

 

I tried to make something using the method you just showed and I had an unexpected outcome. The object seemed to normalize to the curve instead of staying flat to it?


 Hi there,

 

In your case, I'd use a slightly different approach [this method could also be employed on the skateboard deck].....try extruding a surface for each direction [I had to extend the sides of your base in order to intersect cleanly] and then trimmed accordingly.....then thicken and add your other treatments as desired.

 

ORK_SHIELD [ExtrudedSurfaces].png

 

ORK_SHIELD [TrimmedSurfaces].png

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Problem with bending of face

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hello nanan00,

Maybe this video will help.

(view in My Videos)

Cheers

Mark

Re: Problem with bending of face

Legend
Legend

Thank you Sean and Mark.

 

I am still unsure why I was getting that bow in the shape instead of the flat edge when on the skateboard it retained the flat center section.

 

With what I do here at work surfaces rarely come up so I have not had much time or need to look into the how and why of those features.

Re: Problem with bending of face

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
The bow shape was because you created a surface from the outside 3d curve only. The bounded surface had no other information to work from and therefore has no real control of the interior shape.
Cheers
Mark

Sent from my iPad

Re: Problem with bending of face

Legend
Legend

Was that not the same case for the skateboard?

 

 

 

Lessons applied, looks good.

My free time is usually spent drawing all kinds of stuff like weapons and armor, buildings, cars etc. Solid Edge has been a challange to learn but all in all seems like a very strong program.