Cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with converting to sheet

Experimenter
Experimenter

Hello. I can't convert it to a sheet body with oblique angles. Has anyone seen this and knows a solution? SE st10

2018-01-31_13-45-15.png

7 REPLIES 7

Re: Problem with converting to sheet

Gears Phenom Gears Phenom
Gears Phenom

Hi @Shurick

 

quicker would be to create it directly in Sheet metal.

 

In your model, there are some minor issues, especially in the corners.

 

cheers,

Arek

Betreff: Problem with converting to sheet

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Shurick

 

 

 

or without the use of a thinwall feature.

 

You can use the "Part To Sheetmetal" function in Ordered

 

20180131_2003.PNG

regards
Wolfgang

Betreff: Problem with converting to sheet

Experimenter
Experimenter

It is also not working.

2018-02-01_12-18-43.png2018-02-01_12-18-10.png

Betreff: Problem with converting to sheet

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

Unfortunately, you can not use "basic" convert to sheetmetal in your case because of bend angles. But don't worry try to use this method:

 

BR,

Imics
http://solidedgest.wordpress.com/

Betreff: Problem with converting to sheet

Experimenter
Experimenter

Thank you .  This will solve the problem, but is too difficult for frequent use.

Betreff: Problem with converting to sheet

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

That's @Imics's signature style.

He comes in when everyone else has given up and provides an out-of-this-world solutions to nearly impossible tasks.

You are a true Genius my Friend !

Thank you for a wonderful video !!

Betreff: Problem with converting to sheet

Gears Phenom Gears Phenom
Gears Phenom

Yes, you're right! Your model is simple, but the solving is not...

 

BR,

Imics
http://solidedgest.wordpress.com/