Cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with installation of Solid Edge st6 Student Edition

N/A

Hi all,
first of all I must apologize for my English.....it's really dangerous!!!!! Smiley Wink
I downloaded Solid Edge St6 Student Edition,but the installation crashes at first window.My OS is Windows 7 Home Premium,64 bit.I read that Solid Edge support only Windos 7 Enterprise,Professional and Ultimate editions.Is that the problem??And is there a solution?
Thank you all for answer me Smiley Happy

8 REPLIES

Re: Problem with installation of Solid Edge st6 Student Edition

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
Hi there,
You should still be able to install it...there's something else going on.
Try right mouse button clicking on the install file and then choose " Run as Administrator", hopefully you can get it installed then.
Sean Cresswell
Streetscape Ltd
sean@streetscape.co.nz
-
Sent from my Samsung Galaxy S4 using Tapatalk 2.
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP7] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: Problem with installation of Solid Edge st6 Student Edition

N/A
I can't install it either. Once the program finishes extracting it just disappears and stops. I tried 3 times, all with the same result. Can someone help? I tried running it as an administrator also

Re: Problem with installation of Solid Edge st6 Student Edition

N/A
Please help me I received an error you are attempting to install solid edge st6 on a non supported operating system ....

Re: Problem with installation of Solid Edge st6 Student Edition

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
Please help me I received an error you are attempting to install solid edge st6 on a non supported operating system ....

Hi there,
What operating system is your computer running?...
------------
Operating System Requirements and Information
This release of Solid Edge has been certified to run on the following:


    Windows 7 Enterprise, Ultimate, or Professional (32-bit or 64-bit) with
    Service Pack 1
    Windows 8 Pro or Enterprise (32-bit or 64-bit)
    Windows 8 (home) and Windows 8 RT are not supported
    Internet Explorer 10 (IE 8 meets minimum requirements)

Solid Edge stops certifying new releases against an operating system shortly
after Microsoft drops mainstream support for it. Microsoft dropped mainstream
support for XP in April 2009. Microsoft dropped mainstream support for Vista in
April 2012. Solid Edge ST6 does not install on Windows Vista or Windows XP.
----------
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP7] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: Problem with installation of Solid Edge st6 Student Edition

N/A
please help me ! compiling the form on solid edge website i've accidentally selected the wrong version of solid edge (32bit and not 64) and now i can't install it ! what should i do in order to receive another mail with the right version ? thank you very much !

Re: Problem with installation of Solid Edge st6 Student Edition

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
There is only one version for the student download and it is 32 bit which will install fine on both 32 and 64 bit versions of Windows as long as it is Windows 7 or 8.


Ken

Production: ST10 MP6
Testing: SE 2019

Re: Problem with installation of Solid Edge st6 Student Edition

N/A
I tried running as administrator.....but it didn't work.Does anyone had any other ideas???

Re: Problem with installation of Solid Edge st6 Student Edition

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
I tried running as administrator.....but it didn't work.Does anyone had any other ideas???


The problem is probably on the graphic card driver. We had another student with the same problem: crash when the SE start window (NOT the part or assembly window) appears. As soon as we went to Control Panel>Device Manager and disabled the Nvidia driver, SE run fine. So, try to install different drivers (may not be the latest ones, as the drivers are general and may not be the best for your specific card).