Cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with log-in to the Forum

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

I have randomly a problem to log in the the forum with this error :

 


Log in issue.png  

any idea what is this ?

Thank you,

Arek

2 REPLIES 2

Betreff: Problem with log-in to the Forum

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @arekkul

 

refering the IP adress I would assume that this more is an internal problem with Your proxy rather than with the connection to the Siemens server.

 

10.5.1.500 (500 is an allowed number?) shows more to be an internal IP from Your local network.

 

 

 

regards
Wolfgang

Betreff: Problem with log-in to the Forum

Gears Phenom Gears Phenom
Gears Phenom

Hi @hawcad

 

thank you for your response,

 

I will check it internally,

 

Regards,

Arek