Reply

Problem with open dft in viewer ST9

Hi everybody,

 

I have a problem to open a dft in SE viewer ST9 viewer:

If i act double click on the file dft the viewer start, but don't open the file(seems dont load the file), after this i can open the dft file from the viewer, and its work.

 

Has someone  some feedback???

5 REPLIES

Re: Problem with open dft in viewer ST9

I can't open .dft either by double-clicking it nor with "open file" from inside the program...

when I double click, the program starts but it does not open anything, no error message.

 

I'm running SE viewer ST9 with Maintenance Pack 9.

 

The viewer can open .asm and .dxf without problems, just not the .dft

 

(System:  Windows 7 Professional x64)

Re: Problem with open dft in viewer ST9

Hello,

just a quick question: do you have any national characters in dft names?

I think I faced similar issue when national characters (i.e. czech ščřžý) are used in file name.

 

Ota

Re: Problem with open dft in viewer ST9

No, just regular characters. ex file name:   REATRE3660BEQNF.dft

Re: Problem with open dft in viewer ST9

I experimented a bit with the computer, when I try to open a .dft in a different session, it opens. The problem seems to be user related.

Re: Problem with open dft in viewer ST9

Here is what solved the problem for me:

 

 

- open windows explorer and find the folder:

 

C:\Users\<username>\AppData\Roaming\Unigraphics Solutions

 

and rename it to something else like

 

C:\Users\<username>\AppData\Roaming\Unigraphics Solutions_

 

 

try opening your file again by double cliking it.