Cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with open non solid edge document

Experimenter
Experimenter

Hello everybody!
I am a student of mechanical engineering. 
I use the program Solid Edge ST (as the old version). something days ago I had something broken and now I can not open files that are not of solidedge. I reinstall it and delete everything from register and there was no improvement. when I click to open, select the file and then click open, it opened empty dialog box and I can't do anything. 
Here is picture for better understanding. All tabs are empty. 

problem.png

11 REPLIES 11

Re: Problem with open non solid edge document

Gears Phenom Gears Phenom
Gears Phenom
Check in options \ file locations that you template folder is setted correctly.

Re: Problem with open non solid edge document

Experimenter
Experimenter

I checked and it looks good. C:\Program Files (x86)\Solid Edge ST\Template. In this file are saved all templates

Re: Problem with open non solid edge document

Legend
Legend

You need to go to solid edge option, go to Helpers, go to the Set Default Templates, and then set each template location to your templates.

 

Capture.JPG

ST8 MP9
Go FAST, or go home.

Re: Problem with open non solid edge document

Gears Phenom Gears Phenom
Gears Phenom

@BoatTech wrote:

You need to go to solid edge option, go to Helpers, go to the Set Default Templates, and then set each template location to your templates.

 

Capture.JPG


I don't think this option is present in the old ST1

Re: Problem with open non solid edge document

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Can you try copying the files from the C:\Program Files\Solid Edge\Template folder to a temporary location, say C:\Temp then set the path from the Application Options and check again if they are listed in the 'New' dialog. I believe a Solid Edge restart may be required.

 

~Tushar

Re: Problem with open non solid edge document

Experimenter
Experimenter

when I try these it also open empty dialog box :/ 
template1.jpg

Re: Problem with open non solid edge document

Experimenter
Experimenter

Tushar This has helped Smiley Happy thanx a lot!!

Re: Problem with open non solid edge document

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

What operating system are you using?  If memory serves correctly, ST would only work on XP and would have issues with Win 7 protected folder virtualization.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: Problem with open non solid edge document

Experimenter
Experimenter

win7