Cancel
Showing results for 
Search instead for 
Did you mean: 

Problems Installing 2D Drafting on Windows 8 and Windows 10

Siemens Phenom Siemens Phenom
Siemens Phenom

If you have problems installing Solid Edge 2D Drafting on Windows 8 or on Windows 10, it may be as a result of .NET Framework 3.5 not installing properly by the installation process. This is a Microfoft component that is required by Solid Edge 2D Drafting.

 

On Windows 8 and Windows 10 machines, you should manually install Microsoft .NET Framework 3.5 prior to starting the Solid Edge ST8 install. To install .NET 3.5, in Control Panel, open “Programs and Features”, select “Turn Windows features on or off”, then on the “Windows Features” dialog select “.NET Framework 3.5 (includes .NET 2.0 and 3.0)” and OK to install.

 

7 REPLIES

Re: Problems Installing 2D Drafting on Windows 8 and Windows 10

Creator
Creator

Hi;

 

When installing "Solid-edge 107 SE_Free_2D_SPANISH_ST7" installer asks for framework 3.5. 

 

The problem is that we are not able to install framework 3.5,  installer do nothing.

 

Any clue

 

 

Re: Problems Installing 2D Drafting on Windows 8 and Windows 10

Creator
Creator

I forgot to say that the hardware is a

SURFACE PRO 3
 
Regards.

Re: Problems Installing 2D Drafting on Windows 8 and Windows 10

Creator
Creator

 

And opertaing System is w8.1 in spanish.

Re: Problems Installing 2D Drafting on Windows 8 and Windows 10

Siemens Phenom Siemens Phenom
Siemens Phenom

Are you saying that the Installer for Solid Edge does nothing? Or that trying to install the .NET framework separately does nothing?

 

Regards,

Rick B.

Re: Problems Installing 2D Drafting on Windows 8 and Windows 10

Creator
Creator

Hi Rick;

 

.NET framework 3.5 separately does nothing.

 

Regards.

 

 

Re: Problems Installing 2D Drafting on Windows 8 and Windows 10

Experimenter
Experimenter

Hello,

I am trying to install the 2D CAD software for SOlid Edge and I keep getting an error message.

The small box that pops up has  7-zip in the upper left corner and the main texts says:

 

"The requested operation requires elevation"

 

Please let me know what is wrong?

I am installing on Windows 10 with the NET Framework 3.5 installed/turned on.

 

Re: Problems Installing 2D Drafting on Windows 8 and Windows 10

Siemens Phenom Siemens Phenom
Siemens Phenom

Because you are not installing as the administrator user...

 

Right-click on the downloaded exe file and select "Run as administrator".