Cancel
Showing results for 
Search instead for 
Did you mean: 

Problems during instalation proces- extracting

N/A

Hi Everyone!
I have this student version of Solid Edge. I use Windows 7, 64-bit version. When i try to open this file ".exe" it doesn't finish the operation. The name of this application contains: "...32bit.." ,so i think it might be the problem. My question: what can I do about it? Is there any other version of this application- I mean the one compatible whit 64 bit version of Win7?
Thanks for your answers

2 REPLIES

Re: Problems during instalation proces- extracting

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
The one you have is compatible with 64 bit.
Stop your AV product. Right click on it and select "Run as Administrator". Install it to "C:\Solid Edge". If it still fails, you most likely have a corrupt download... download it again. Best to use a download manager like ZAP.


Ken

Production: ST10 MP6
Testing: SE 2019

Re: Problems during instalation proces- extracting

N/A
But, i don't know if it is possible to download this programme (using the same or new link from Siemens) again. I think, that will be difficult cause the Company might think that I want to wheedle second programme for the same person or sth... I don't know what to do. Is there any chance to dwonload it once again?
Thanks in advance