Cancel
Showing results for 
Search instead for 
Did you mean: 

Problems making the correct dimension (from hole to edge of plate)

Valued Contributor
Valued Contributor

Hi,

 

I have problems dimensioning the distance from the hole to the edge.

I would like to know how much the hole has been "offset" from the edge.

 

3 REPLIES 3

Re: Problems making the correct dimension (from hole to edge of plate)

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hi,

 

I'd suggest using Distance Between instead of Smart Dimension along with the steering wheel.

If the hole is already placed, use a coordinate system with one axis aligned to the inclined edge and dimension the hole center with the axis.

 

 

~Tushar

Re: Problems making the correct dimension (from hole to edge of plate)

Valued Contributor
Valued Contributor

Cant get that to work Smiley Sad

 

 

Highlighted

Re: Problems making the correct dimension (from hole to edge of plate)

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,


okay, first of all, I think that there is a big change between ST6 what Tushar is showing and ST8 what we use.

 

The standard behaviour of Solid Edge using distance dimension between 2 points doesn't work proper when using edges instead of 2D sketch lines.

At least here with ST8

 

So the only solution I can give is, that You use the method "dimensions axis" instead (what is seen in Your video already) but You have to define the dimension axis using the small icon on the left of the toolbar, selecting You reference axis

 

Then it work as it should, but I think the 2 ponits method must be adapted to be in the same way as in 2D sketches.

 

Here is the video:

 

This video is currently being processed. Please try again in a few minutes.
(view in My Videos)

 

 

regards
Wolfgang