Cancel
Showing results for 
Search instead for 
Did you mean: 

Problems to orient the dft to pint it

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hello!

 

I'm tring to pint dft with the ST10 version and I found some problems. The dft appears 90º rotated on the pdf and on the sheet printed.

 

I have the options shown in the image selected. 

 

I tried it with different printers and without MP, with the MP1 and with the MP2 in the ST10 always.

 

I didn't had any problem printing with the ST9.

 

Any idea??

 

Thank you!

3 REPLIES 3

Betreff: Problems to orient the dft to pint it

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @BeatrizSeoane

 

 

 

do You PRINT the draft using any PDF printer driver or do You save the draft as PDF?

 

These are two different issues and actions with seperate settings.

 

Best IMHO always is to save as PDF using the internal SE postscript printer

 

And this one should bring Your papers to the right orientation.

 

regards
Wolfgang

Re: Problems to orient the dft to pint it

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

This is a known issue... This will be fixed next version of Solid Edge.

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: Problems to orient the dft to pint it

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Imics

Hi @BeatrizSeoane

 

 

so now I'm out of mind.

 

What is the issue?

This is what I haven't understand.

 

To print a Solid Edge draft to PDF and to have the correct paper siz?

 

I just tested a 3 page draft with 3 different paper sizes on each page.

What I get as result is a PDF with 3 pages with different paper size for all of them.

 

So please might You explain what You want to get and where the problem is, this would be great - thanks

 

regards
Wolfgang