Cancel
Showing results for 
Search instead for 
Did you mean: 

Programming in Windows 2008 r2 RPC problems

Experimenter
Experimenter

Hello:

Some months ago I developed an application on vb.NET that opens SE proyects and prints them automatically. It works perfectly on Windows XP machine. But since I moved the application to Windows Server 2008 r2, I'm getting "RPC server is unavailable" error sometimes, usually on document closing or on sheet activation. I have Exceptions to catch this error and also OleMessageFilter class, but it's not working. Before the exception is caught, appears the "Solid Edge has encountered an error and needs to close" window.

 

The application restarts SE when 200 documents have been opened, and calls Garbage Collector every time a document is closed.

 

Thanks

 

1 REPLY 1

Re: Programming in Windows 2008 r2 RPC problems

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Server OS's are not supported for Solid Edge.



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com