Cancel
Showing results for 
Search instead for 
Did you mean: 

Project curve from cylinder to cylinder

Experimenter
Experimenter

Hi everyone Is there any way i can project a curve from a cylindrical face, to an other cylindrical face, same diameter, but not the same modell, its an assembly.
I want to project the port from the gray model to the blue surface:
asd.pngSorry for my bad english, its not my motherlanguage... Smiley Sad

2 REPLIES 2

Betreff: Project curve from cylinder to cylinder

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @techni

 

 

I would say, since it ist the same diameter, it is the same cylinder face.

And therefore you can copy the cylindrical surface, which also includes the curve (face region) for a later use.

 

You can do this via assembly and interaprt copy from one part to another or also via part copy.

However You prefer to do.

 

 

regards
Wolfgang

Betreff: Project curve from cylinder to cylinder

Experimenter
Experimenter

Thank you, its worked. I would never find out myself. So thx again.
asd2.png