Cancel
Showing results for 
Search instead for 
Did you mean: 

Project to Sketch (ST8 & 9) Non-associative

Gears Phenom Gears Phenom
Gears Phenom

Before I start, I found this post a few years back with the same problem, but doesn't have any solutions.

https://community.plm.automation.siemens.com/t5/Solid-Edge-Forum/Project-to-Sketch-Options/m-p/34856...

 

My coworker and I both -- 2 different user profiles, 2 different computers, 1 ST8, 1 ST9 -- can't get the Project o Sketch options to allow associativity.

Project to Sketch.png

All of the Inter-Part links options are checked in the Solid Edge Options.

 

The part that we have an issue with is a mix of Synchronous and Ordered features.  The sketch we are trying to project an associative edge to is within an Ordered feature.

 

I'm at a loss to figure out why the option is greyed out.


____________________________________
--Scott Wertel, P.E.
8 REPLIES

Re: Project to Sketch (ST8 & 9) Non-associative

Honored Contributor
Honored Contributor

I have run into the same thing. Never figured out exactly why. Sometimes I had to re-make the part, other times I did get past it but don't remember how. I think it had to so with the sequence of events in ordered. IE one of the part's that the sketch is realted to moved to later in the sequence.

Re: Project to Sketch (ST8 & 9) Non-associative

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

This can happen if the part is being edited out of context.

Re: Project to Sketch (ST8 & 9) Non-associative

Gears Phenom Gears Phenom
Gears Phenom

The part is being edited in-context, accessed through the Right-Click -> Edit menu.


____________________________________
--Scott Wertel, P.E.

Re: Project to Sketch (ST8 & 9) Non-associative

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @swertel,

 

Is it by chance, an edit within a sub-assembly, that in turn was from an edit in a top level assembly?.....

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Project to Sketch (ST8 & 9) Non-associative

Genius
Genius

Hi

 

I have also had this problem intermittently, over many years. Never really found the reason, but at one stage I was thinking it was something to do with if 'Project to Sketch' had previously been used in the part and, if it had, redoing the previous projections and then the Associative button would be selectable.

 

I would love to have a definate solution to this. 

585 ST10 Win 7

Re: Project to Sketch (ST8 & 9) Non-associative

Gears Phenom Gears Phenom
Gears Phenom

@SeanCresswell The only subassembly in this file is the part that the tool is designed around.  All interpart links are between the tool's components, so they all exist at the top level.


____________________________________
--Scott Wertel, P.E.

Re: Project to Sketch (ST8 & 9) Non-associative

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

How about Application Button>Options>Inter-Part>Project to sketch...?

LMGi
www.TLMGi.com

Re: Project to Sketch (ST8 & 9) Non-associative

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

What happens if you create an inter part copy while editing that part?  Does that work?