Cancel
Showing results for 
Search instead for 
Did you mean: 

Properties Manager changes material of all parts

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

In an assembly I'm using Inspect/Properties Manager to change material of parts.

Disconcertingly when I change the field for one part it changes the material for all parts.

This doesn't seem like the desired default behavior. I would think one would be able to use it to change material for selected parts. If you want the same material for all parts you change one then copy/paste into the others.

Maybe someone with earlier versions of SE can check the functionality and tell me if it's the same.

This video is currently being processed. Please try again in a few minutes.
(view in My Videos)

Bruce Shand
ST10 MP7 - Insight - Win10 - K4200
7 REPLIES

Re: Properties Manager changes material of all parts

Valued Contributor
Valued Contributor

Mine works ok. 

Just installed MP2 , maybe it has been corrected. good luck

Re: Properties Manager changes material of all parts

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@AlexBergeron, By "OK" do you mean you can change a part's material and the others in the list don't change?

Bruce Shand
ST10 MP7 - Insight - Win10 - K4200

Re: Properties Manager changes material of all parts

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,

no, only that single part I seleted has changed it material.

Just as I wanted it to do

 

 



regards
Wolfgang

Re: Properties Manager changes material of all parts

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

OK, I just noticed that while changing one part material and having the same material show up for all the changeable parts shown in the properties manager is an illusion. When you close and reopen the properties manager dialog only the part selected is actually changed.

Not good. @AlexBergeron, is that what you see with MP2?

@hawcad, what version and MP are you on?

Bruce Shand
ST10 MP7 - Insight - Win10 - K4200

Re: Properties Manager changes material of all parts

Valued Contributor
Valued Contributor

No, only the one selected change as expected. 

Re: Properties Manager changes material of all parts

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,


I have running ST8 with MP2 here too

 

 



regards
Wolfgang

Re: Properties Manager changes material of all parts

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@hawcad, OK, so the other parts don't show changed in the list like in my video? Only the part selected? If so, it must be an MP2 fix.

Bruce Shand
ST10 MP7 - Insight - Win10 - K4200