Cancel
Showing results for 
Search instead for 
Did you mean: 

Property Manager Preview - Turn This Off?

Pioneer
Pioneer

Hi,

 

This is a minor petty issue that probably doesn't warrant it's own thread but I can't find a solution online anywhere.

 

When I open Property Manager in an assembly, I get a File Preview appear, in the same annoying place every time nomatter where I move it or how many times I click "X".

 

Is there any way to turn this off entirely or get the software to remember I want it off?

 

I don't see any options on the Property Manager anywhere.

 

See attached for what I mean. "OK" "Cancel" and "Help" are obstructed.

 

Thanks

6 REPLIES 6

Betreff: Property Manager Preview - Turn This Off?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @User_Error

 

 

 

Yes indeed this is one of those "big issues" which can frustrate one!

 

As often as You open the Property Manager You will get this preview window.

Which itself is not bad, but always at the worst position and place on screen.

And there is no learning effect of where it should stay!

 

I think this also is a point for the "Call for Pet Peeves 2.0"

 

 

regards
Wolfgang

Betreff: Property Manager Preview - Turn This Off?

Pioneer
Pioneer

@hawcad

 

Is there a thread for Call for Pet Peeves 2.0? Sounds like something that would be useful now ST10 has been out a while with a few service packs.

 

I hope the SE developers check these threads, it's such a small simple thing to fix that would make the User Interface much less annoying. Just need a simple "Options" button like in Design Manager where you can turn tool tips off (per attached).

Betreff: Property Manager Preview - Turn This Off?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @User_Error

 

 

 

 

 

Yes there is  a thread "Call for Pet Peeves" but No this is not the place to bring ideas to the developement.

This only can be achieved opening an ER call at GTAC or via Your Siemens partner!

 

Thats the only and good way to enhance the software!

 

regards
Wolfgang

Re: Property Manager Preview - Turn This Off?

Valued Contributor
Valued Contributor

Hi,

 

There is indeed a way to turn the preview off;

 

Look at the top left hand corner, you will see an icon marked preview.

Select this to either turn on or off.

DM will remember the setting.

 

 

Matt Hunt IEng.MIED
Design Engineer
M-Flow Technologies

ST10 MP*
K2200
Highlighted

Re: Property Manager Preview - Turn This Off?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @MattHunt

 

 

 

Yes will work for Design Manager, but we talked about Property Manager!

And unfortunateley there is no option for turning on/off the preview in PM.

regards
Wolfgang

Re: Property Manager Preview - Turn This Off?

Valued Contributor
Valued Contributor

Ah!

 

That will teach to read first eh?

Yep you're quite right of course.

Matt Hunt IEng.MIED
Design Engineer
M-Flow Technologies

ST10 MP*
K2200