Cancel
Showing results for 
Search instead for 
Did you mean: 

Property Manager

Legend
Legend

Sometimes when I go through property manager to update stuff, it doesn't save. Now, the save button never seems to work, so I have no idea if my updates are going to save. I'm doing something wrong, any suggestions? I open property manager from the assembly.

 

Help me Ol' Wise ONes!

ST8 MP9
Go FAST, or go home.
12 REPLIES 12

Re: Property Manager

Legend
Legend

If you open Propert Manager from a part or assembly file, the save button is not active. Make your changes, close the Property Manager and then save your part or your assembly.

If you don't save and close, SE won't prompt you to save and your changes are lost.

Greetings from Germany
Christian Kunkel
https://c-k-m.info
Highlighted

Re: Property Manager

Legend
Legend

Hmm, lost all my updates from property manager when I closed it, and then saved my assembly...........

ST8 MP9
Go FAST, or go home.

Re: Property Manager

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@ckunkel72 wrote:

If you open Propert Manager from a part or assembly file, the save button is not active. Make your changes, close the Property Manager and then save your part or your assembly.

If you don't save and close, SE won't prompt you to save and your changes are lost.


When I change properties in a part or assembly, and it's the only change, I do get a prompt to save.

And the save button is always active.

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Re: Property Manager

Legend
Legend
In Property Manager you have an active Save button? Mine never is active, even after going through and making multiple changes in Property Manager. I closed Property Manager, and then went right to save my assembly, but none of the information I entered into Property Manager existed.
ST8 MP9
Go FAST, or go home.

Re: Property Manager

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

No, I don't have a save button in Prop Man at all so I don't even know what you mean. I assumed you guys were talking about the file save button.

Other than that stuff I put in in Prop Man is retained. We use Prop Man all the time.

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Re: Property Manager

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

Save button of Property Manager is active when you use PM under System button without opened document.

 

Here is a short video:

 

BR,

 

Imics
http://solidedgest.wordpress.com/

Re: Property Manager

Legend
Legend
Thank you very much Imics, that's the answer I was looking for!
ST8 MP9
Go FAST, or go home.

Re: Property Manager

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@BoatTech  You said you opened PM from an assy. Imics talked about using PM without an open assy.

So what was the actual problem in the first place and how was it resolved?

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Re: Property Manager

Legend
Legend

Opening from the assembly doesn't make the Save button active. I didn't know you could go to Property Manager through the main screen, without opening the assembly.

 

Capture.JPG

 

Yesterday when I was working through this, I was able to change materials via the Property Manager. For some reason, opening from the main screen, I don't have the option to change materials.

ST8 MP9
Go FAST, or go home.