Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Property Manager

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I can change material on parts (not assys, of course) in stand-alone PM but it doesn't have the nice drop down menu.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Property Manager

Legend
Legend

Well, what the flick? I have the ability to change materials when opening PM via the assembly:

 

Capture.JPG

 

But, when I open PM from the main screen, the same assembly doesn't have the ability to change materials:

Capture2.JPG

ST8 MP9
Go FAST, or go home.

Re: Property Manager

Legend
Legend
The file has to be active to change the material. I just ran into this the other day. Also when I open PM from an assembly there is no save button, you close it with the OK button to accept your changes. I always save the file right after. I lost changes by not doing that back in the dim reaches of time and I've done it ever since.
Using SE since V12, 2002
ST10 certified