Cancel
Showing results for 
Search instead for 
Did you mean: 

Property display

Honored Contributor
Honored Contributor

Let's say I have a property L with a current value of 6.125

 

I can easily control the display from 0 to 3 decimals. But this is a fixed result.

 

In some cases in the parts list (not the one above) I have dynamic display but I'm not sure what controls or created that.

 

What I mean by dynamic display is:

if L=6; 6 is displayed

if L=6.125; 6.125 is displayed

 

as apposed to 0 digits where:

if L=6; 6 is displayed

if L=6.125; 6 is displayed

 

or 3 digits where:

if L=6; 6.000 is displayed

if L=6.125; 6.125 is displayed

 

What formatting or situations creates the dynamic display?

5 REPLIES

Re: Property display

Legend
Legend

I have been looking for such myself. Where did you see the dynamic display in Solid Edge?

Re: Property display

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Not sure what you mean but - units precision?

Bruce Shand
ST10 MP7 - Insight - Win10 - K4200

Re: Property display

Honored Contributor
Honored Contributor

How can I explain this better?

 

Two cases:

case 1, x=6

case 2 x=6.4375

 

In case 1, I want 6 to display (NOT 6.000)

in case 2, I want 6.438 to display

 

how do I get that done?

 

I currently see this behavior with:

Flat_Pattern_model_CutsizeX

Flat_Pattern_model_CutsizeY

I did not do anything to get that done, it just is that way in the parts list.

However, I think I cheated. I only left room for just under 4 characters(and a decimal) to display. It could be trying to display 7 digits past the decimal, and I did not allow that room to show up.

 

 

Re: Property display

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Oh, so like in a dimension where you can turn off trailing zeroes? I don't know how to do that or if it can be done with property values in a parts list.

Bruce Shand
ST10 MP7 - Insight - Win10 - K4200

Re: Property display

Honored Contributor
Honored Contributor

Bingo. This is for the purpose of saving room. I draft everything on A size paper, Every 1/16" of an inch on paper is valuble.

 

unrelated: I hope the hole table can vary in height in ST8. That missing control costs me extra pages much of the time just to display a hole table.