Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Property text code: where to find them?

Valued Contributor
Valued Contributor

Dear friends,

I would like to have a table with all the property adn symbol text code for ST10, is it possible to find it somewhere?

 

Thanks for your help!

13 REPLIES 13

Re: Property text code: where to find them?

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Here is a link to the property text codes in the help file for ST10

 

Property Text Codes

Re: Property text code: where to find them?

Valued Contributor
Valued Contributor

Thanks @bweisenberger,

but there are other codes, like for example "@2|" for truncate a dimension measure like this:

 

%{Materiale|R1}
%{Flat_Pattern_Model_CutSizeY/@2/CP/NU|R1} x %{Flat_Pattern_Model_CutSizeX/@2/CP/NU|R1} x %{Spessore/@2|R1}

 

Is it possible to find them all?

 

thanks!

Re: Property text code: where to find them?

Valued Contributor
Valued Contributor

I answer to myself Smiley Very Happy

They are in this page!

 

Re: Property text code: where to find them?

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

A lot of those values can be found when using the Format button on a callout. Simply click the callout text (in this case %HC) then click the Format button below and you can select most of the options you were asking for. 

 

Capture.JPG

Re: Property text code: where to find them?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Davide_Parolin

 

 

no need for knwoing them all - as it was in earlier times.

Now You simply can formate all Your property text using the integrated and graphical format style form.

 

 

20180403_1510.png

regards
Wolfgang

Re: Property text code: where to find them?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @bweisenberger

 

 

 

sorry for posting the same answer after Yours, but I have started to answer, and then the phone has rung keeping me away from pushing the send button

 

regards
Wolfgang

Re: Property text code: where to find them?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Any idea why the format button is greyed out here?

 

CalloutFormat.JPG

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Property text code: where to find them?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @bshand

 

 

 

click into the callout code, then the Format button should get active too!

 

regards
Wolfgang

Re: Property text code: where to find them?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

OK. Not a very good interface IMO but no matter.

So now why is this format values page greyed out?

FormatValues.JPG

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200