Cancel
Showing results for 
Search instead for 
Did you mean: 

Pull with force?... or something else

Valued Contributor
Valued Contributor

Hi,

 

How can I make the "arm" pull to the left, so it will connect with the flange?

 

We are going to connect a spring between the 2nd hole and a bracket (in the cover) - this will force the arm to connect with the flange - not sure if that is possible with SE.

 

I made a small video to show my problem:

 

, Kenneth

4 REPLIES 4

Betreff: Pull with force?... or something else

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Kenneth

 

 

I would like to say, that this will not be possible with standard SE functions, maybe with additional construction surfaces and extra relations.

 

It could be worth to take a look into Simply Motion.

There springs can be defined as well as contacts.

 

But all has to be considered more in detail.

regards
Wolfgang

Betreff: Pull with force?... or something else

Valued Contributor
Valued Contributor

Thanks for the reply.

What kind of extra relations would you recommend?

 

Betreff: Pull with force?... or something else

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

HI @Kenneth

 

I can imagine that a Path relation will do that for You!

 

Connect the outest edge of Your arm to the edge path of Your flange 

 

 

I just tested this with a different assembly where YOu can connect a line/edge to the chained edge of another part and now You can move that along it.

 

Maybe it is not 100% exact in Your case, if not only the edge is touching the flange, but then YOu have to use a Cam relation

 

 

regards
Wolfgang

Betreff: Pull with force?... or something else

Valued Contributor
Valued Contributor

Good suggestion, I will try that Smiley Happy