Cancel
Showing results for 
Search instead for 
Did you mean: 

Purge Blocks

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Some one had asked for this a while ago but I am unable to find which post.

The attached macro purges i.e. deletes all un-used blocks

These are blocks which have no occurrences placed in the Draft.

 

The command has roots in an equivalent feature in AutoCAD where people use it for reducing the file size.

Other similar references are Purge Layers, Purge Variables and Purge CFG files.

 

~Tushar Suradkar

fb.pngSolid Edge Users Facebook Group

6 REPLIES 6

Re: Purge Blocks

Gears Phenom Gears Phenom
Gears Phenom
Thnx my Friend! I'm going to test it.

BR,
Imics
http://solidedgest.wordpress.com/

Re: Purge Blocks

Gears Phenom Gears Phenom
Gears Phenom

@Tushar I've tested it and it works well in ST9. Thnx!

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: Purge Blocks

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Thanks for the test @Imics

I hope it will be useful for people migrating from AutoCAD to Solid Edge.

   

~Tushar

 

Re: Purge Blocks

Experimenter
Experimenter
... does what i should in ST6 - thx a lot!

Re: Purge Blocks

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Thanks for confirming in ST 6

Re: Purge Blocks

Experimenter
Experimenter

would it be possible to purge the unused blockviews too?

as you see in the image below, after i have executed your tool, in the blockgroups are many unused views left over. is there a way to purge this too with your tool?

SE-ST6-unused-blockviews-in-blocks.pngpurge unused blockviews too