Cancel
Showing results for 
Search instead for 
Did you mean: 

Question Mark In Pathfinder

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

As soon as I open a document there is a window that shows load failure with these part in pathfinder

I've tried to delete all the parts at once, tried single attempt nothing.

The only thing I can think of my computer crashed while moving a part.

 

Thank You

Greg

1 REPLY

Hi Greg,   What Solid Edge is saying by "Load Failure" is...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi Greg,

 

What Solid Edge is saying by "Load Failure" is it can nolonger find the part[s] that are links only, to the original files, and you need to restore them.....this is usually best handled by using revision manager, but, replace part and manage links can also be used to varying degrees of difficulty dependant on the number of unique parts that need restoring/replacing.

Now that you have deleted them from the pathfinder, you have no choice but to re-do the entire assembly, by placing the part[s] again.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x2 seats]
Windows 10 - Quadro P2000