Quick View Cube has disappeared

Valued Contributor
Valued Contributor

I have tried to activate it from the options menu.

Do I have to activate it somehwere else?

 

ST9
Surface Pro 4
2 REPLIES

Re: Quick View Cube has disappeared

Esteemed Contributor
Esteemed Contributor

That's the right spot.  Looks like it's an issue with your graphics card and the settings that SE automatically uses with it.  I was able to reproduce it not displaying by switching the Solid Edge Application Display setting to "Graphics Card Driven (Basic)" which is what your picture is showing.  Looks like it is dependent on using the Display Lists which is only available using the "Graphics Card Driven (Advanced)" setting.


Thanks,
Ken

Production: ST9 MP10
Testing: ST10 MP3

Re: Quick View Cube has disappeared

Valued Contributor
Valued Contributor

Thank you Ken :-)

 

Cube is back and the rendering is faster and better!

 

Cheers,

Geir

ST9
Surface Pro 4