Quickest way to trim and convert to sheet metal.

Builder
Builder

Hello,

 

I want to see if anyone has a better method to do this. The goal is to remove the 0.030" of plasitsol from the part including from the slots and holes and convert to sheet metal in either synchronus or ordered.

 

Thanks,

 

D.L.B.

3 REPLIES

Re: Quickest way to trim and convert to sheet metal.

here's my 5 min stab.  i have to run tonight but if not answered i'll try again in the morning...

 

there is something keeping this from flattening...

 

might need to use the top face and make a new virgin part...

 

see video...: http://screencast.com/t/yYXUVYwrwYp

Re: Quickest way to trim and convert to sheet metal.

SeanCresswell 2nd Gear
2nd Gear

Hi there,

 

Much in same vein as Matt.....however, I noticed for the offset [if you increase the units precision] the distance is actually 0.0295".

I only managed this in Ordered, as I was unable to complete it in Synchronous [in the 2 minutes I gave myself] to a flattened model, for some strange reason.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP3] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: Quickest way to trim and convert to sheet metal.

Sean was right...  you .030 offset was the issue...  see my video attached

 

the offset is .75mm

http://screencast.com/t/brUzAvHJ6

attached is your file which does flatten

 

regards