Cancel
Showing results for 
Search instead for 
Did you mean: 

R1 vs R99

Honored Contributor
Honored Contributor

Is there any way to get a report of the what is R1, R2, etc.... so I can find when in the sequence a specific assembly/part was inserted?

2 REPLIES

Re: R1 vs R99

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Based on your other question you posted, I'm assuming we are talking about a Draft and the sequence models were inserted as drawing views and then using property text "indexed reference".

 

There is no way I know of to get an actual "R1, R2, etc..." list, however if you use the Manage Links dialog, I believe it list the models in the order that they were attached and it updates correctly as views are deleted and added.  So just count down the list until you find the model you want and you should have the correct index number.



Ken
Production: ST10 MP7, Testing: SE 2019
http://Grundey.blogspot.com

Re: R1 vs R99

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,


I suppose that the order could be seen in the Manage Links form in Solid Edge

 

Just did a test and the entries are in exactly that orer I put them into the draft

 

 

20151203_1730.PNG



regards
Wolfgang