Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

RAL Classic colour palette for face styles

Siemens Phenom Siemens Phenom
Siemens Phenom

Recently had a request for a RAL Classic colour palette for face styles.  Although Solid Edge currently does not provide an OOTB RAL colour palette it is possible to create your own custom RAL colour palette.

 

screenshot.418.png 

 

Attached is an ST6 part file and material library containing face styles for the RAL Classic colour palette.

 

All face styles were derived from converting the associated RGB values for each colour.

The RAL Classic colour palette RGB values were taken from http://www.e-paint.co.uk/Lab_values.asp

 

[had to zip the material.mtl file as it is a blocked file extension]

13 REPLIES 13

Re: RAL Classic colour palette for face styles

Valued Contributor
Valued Contributor

I know I'm bumping an old post, but I have a couple of questiions about this:

 

1. How was this created?  This contains over a 100 face styles.  Surely these weren't entered one a time (via Styles > New), as that would have been very time consuming.  But I'm not aware of any automated way of doing this.

 

2. If I want to have different face style "libraries", can I just create separate *.mtl files for each library? I assume then I would just use the style organizer to copy over the one I want to use.

 

I actually have a need for this right now and have been struggling with how best to define and organize different color palettes.  So I'm anxious to learn how this was done.  Thanks!

 

 

Re: RAL Classic colour palette for face styles

Siemens Phenom Siemens Phenom
Siemens Phenom

Actually there was quite a bit of work that went into creating all 213 face styles.

 

Firstly I had to find a resource listing all of the RAL colour names and RGB codes.

 

I then dumped that web page out to an Excel file.

 

After cleaning up the Excel file I then had to create an Excel macro to convert all 213 RAL colour codes from RGB to Solid Edge colour codes.

 

I then dumped the converted spreadsheet out to a text file.

 

I then wrote a macro to read in the values of the RGB colour names and codes from the text file into Solid Edge and create the face styles in the material library.

Re: RAL Classic colour palette for face styles

Gears Phenom Gears Phenom
Gears Phenom

@uk_dave

 

I love this sentence from you:

"After cleaning up the Excel file I then had to create an Excel macro to convert all 213 RAL colour codes from RGB to Solid Edge colour codes"

 

Why doesn't Solid Edge use "standard RGB codes"? Man Frustrated

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: RAL Classic colour palette for face styles

Siemens Phenom Siemens Phenom
Siemens Phenom

Because then I wouldn’t have job security creating solutions such as this Smiley Wink

 

But seriously, I have no idea why Solid Edge doesn't use standard RGB codes.  Most probably legacy code and it would take an effort to update, an effort that at the end of the day would most probably provide minimal return.

Re: RAL Classic colour palette for face styles

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@uk_dave wrote:

Because then I wouldn’t have job security creating solutions such as this Smiley Wink

 


 

....OMG, I litterally sprayed coffee at that! Robot LOL

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: RAL Classic colour palette for face styles

Gears Phenom Gears Phenom
Gears Phenom

Smiley Wink

 

What company is your employer? Smiley Very Happy

 

Thnx my friend!

 

BR,

 

Imics
http://solidedgest.wordpress.com/

Re: RAL Classic colour palette for face styles

Good work, We have the RAL colours for years now but they are a bit old with the colours.

-------
Daniël Schuiling

Re: RAL Classic colour palette for face styles

Double check, the colours are the same. But you have the names behind it, so that is more helpfull. So thank you very much. Kudo given Smiley Wink

-------
Daniël Schuiling

Re: RAL Classic colour palette for face styles

Experimenter
Experimenter

Hi. I can't find the attachment. Can you help me? Thank You.