Cancel
Showing results for 
Search instead for 
Did you mean: 

Re-assign Alt-A to Alt-F

Honored Contributor
Honored Contributor

Is there a way to re-assign Alt-A to Alt-F ?

I'm not sure why, but the File menu is now the Aplication menu. I would like to make it the file menu like all the rest of the programs I use.

 

Then I want to make save an S after using Alt-F. Like every other program I use.

5 REPLIES

Re: Re-assign Alt-A to Alt-F

Genius
Genius

Not sure if you can, but Ctrl+S is "save" in just about every program out there.

Re: Re-assign Alt-A to Alt-F

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Even if you get to somehow change the Alt-A to Alt-F, still would be out of luck.

Further, you need to press SA (replace with F, say) and then another S only to reach Save All.

 

I don't see any way you can get to save using just an S (or F) without getting rid of the Save All sub-menu.

 

01.png

 

02.png

 

Ctrl+S is also a standard and available with Solid Edge. You can try using that.

Though I agree to and contend that menu based shortcuts are logical and easier to remember than random key combinations.

 

~Tushar Suradkar

fb.png

Solid Edge Users Facebook Group

Re: Re-assign Alt-A to Alt-F

Honored Contributor
Honored Contributor

I have used the following hotkeys literally about 1 million times each because MS office and Adobe and AutoCAD all use them. Trying to set up SE the same way.

 

Alt-F-S=save

Alt-F-O=open

Alt-F-A=save as

Alt-F-X=close, no save

 

If I cant get those to work, I use the mouse and menu.

 

Old habits are difficult to break. especially when they have been committed to muscle memory for 30 years.

 

I thought using those hotkeys was a windows requirement.

Re: Re-assign Alt-A to Alt-F

Genius
Genius

These are the same for every windows program...

 

Ctrl-S - Save

Ctrl-O - Open

Ctrl-N - New

 

....No "Save as" I can recall exept for F12 for Microsoft products

Re: Re-assign Alt-A to Alt-F

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

"Old habits are difficult to break. especially when they have been committed to muscle memory for 30 years." - What a wonderful statement !!  @12GAGE 

 

That's absolutely true. All MS Office programs, AutoCAD and Inventor too have taken care that all older Alt+ KB shortcuts are retained with the migration to the ribbon UI.

 

SW has gone the extra 1.6 km in that pressing Alt displays the older pull-down menu in place of the 'Quick Access' menu on the title bar - very elegant. So old users can continue using the menu system and the ribbon is also available all the time.

 

Solid Edge has missed this precious 'Golden Hour' so far. Not necessarily AutoCAD users migrating to SE but current Office users should have been considered. MS Excel users use keyboard the most of any other software. They sure would be using SE too and will definitely won't feel at home in the Golden Hour when it comes to menu based KB shortcuts.